Other Parts Discussed in Thread: LM3423, LM3423BS2LYEV
Tool/software:
Hello, Ti teams.
I intend to drive LEDs at 48 V and 1.2 A output via the LM3421 from a 24 V, 2.5 A input.
The LEDs are connected in series (15 LEDs × 2.8 V Vf = 42 V total).
I want to maintain 100 % output at all times without dimming, and I’m wondering if using the configuration shown in the attached schematic will cause any issues.
I have purchased the LM3423 EVB for testing, but the LEDs didn’t turn on unless a PWM signal was applied. Is a PWM input mandatory?