Tool/software:
It may be useful to perform a full power cycle of the AM335x initiated via software control of the TPS65218D0 PMIC from the AM335x using the I2C interface. Is this possible in the TPS65218D0?
I see the push button input can perform such a function in the "RESET" section 5.4.5 in the TPS65218D0 datasheet, and it seems like such a thing would be useful to trigger from the CPU over I2C, but i don't see that directly implemented, and I don't see a clear means of utilizing the existing register set to do so.