This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24125 STATx Timing

Hello

Do you have some timing and state about the STATx?

1) (Charge state) CE="L"  -> STAT1="L" (max.)

2) (Charge stop) CE="L" -> STAT1="H" (max.)

3) (Charge state) STAT1="L" and STAT2="H" -> (Charge done) STAT1="H" and STAT2="L"

   In this case, STAT1=STAT2="H" or STAT1=STAT2="H" status in the middle of this transition are there?

4) If CE is "H", are the both STAT1 and STAT2 are "H"?

Regards,

PAN