Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
HELLO
I have a gauging problem in the golden image made by the previous made, so I'm currently making a new golden image after looking at the 'slua903_Acheving The Successful Learning Cycle' document.
I think making the learning cycle is over now that the update status has changed to 06, but I have some questions here.
1. At the 5.Conclusion entry in the document, it says to change the update status to 02 before saving the golden file.
1-1) Is the golden file a golden image?
1-2) Update status is not changed to 06 -> 02 is there any way?
2. Is there a way to review the validity of the Golden Image created?
(The gauging was weird on batteries with golden images made before. For example, the gauging changes to 87% ->100% in 3 minutes or 17% -> 0% in 1 minute)
Regards,
ChaeWoo