This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Schematic, pinout and pin functionality guidance.

Part Number: BQ76952

Tool/software:

Hi Team, 

I am planning on not using the AFE's following functionality

1. External MOSFET control.

2. AFE's internal regulator to power other ic's on the board.

3. Fuse cutoff control.

For that I have identified that the following pins can be safely terminated as mentioned in the unused pin section(16.6) of the datasheet.

The following are the pins that I have terminated appropriately as mentioned in 16.6 section, 

29 - CFETOFF

30 - DFETOFF

31 - DCHG

32 - DDSG

34 - REG2 (NOT USING THE INTERNAL REGULATOR TO POWER OTHER IC)

35 - REG1 (NOT USING THE INTERNAL REGULATOR TO POWER OTHER IC)

36 - REGIN (NOT USING THE INTERNAL REGULATOR TO POWER OTHER IC)

37 - BREG (NOT USING THE INTERNAL REGULATOR TO POWER OTHER IC)

38 - FUSE (NOT PLANNING TO USE)

39 - PDSG

40 - PCHG

43 - DSG

45 - CHG

46 - CP1

Could you please let me know if these are all the pins that are not necessary anymore or should any additional pins also be included ?

Thanks, 

G Karthik.