This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1641: output discharge when EN pin is pulled low.

Part Number: TPS1641

Tool/software:

When using TPS16416, and driving it's EN/SHD# pin Low, will the output discharge without external load?

while the datasheet provide information about the output behavior during overcurrent and overvoltage events, I could not found information regarding the output behavior when the EN pin is driving low.

using PSpice simulation module show that the output will discharge without any external load In about 7mSec for 28v (attached pics).

but I would like to confirmed that this is indeed the output behavior. 

Please advise.

Best Regards,

Or Binyamin