This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25306: BQ25306 not charge at above 400mA with different RCHG Resister

Part Number: BQ25306

Tool/software:

I am using bq25306 charging ic in my project for 8.4V battery and I try to charge my battery at above 1A.So, I changed the RCHG resister value 37.2K but my circuit produce at 400mA .

At 20k-400ma only produce 

At 15k-400ma only produce

Changed different RCHG Resister but my circuit produce only 400mA

Vbus=12V -IBAT 280mA

Vbus =9V- IBAT 400mA

I am using 2.2uH inductor (SWPA5040S2R2NT)

Please help me my circuit did not charge 8.4V battery in above 400mA

  1. I am trying different battery with diff PCB but problem not solved