This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: How Can I Keep the Internal Switch for the Thermistor Divider Network Closed All the Time?

Part Number: BQ76952


Tool/software:

We have configured TS1 / TS3 as thermistor inputs. We are using a Semitec-103AT, and have the BQ76952 measurement loop speed to 126 ms. For testing purposes, we would like to observe, with high precision using a multimeter, the voltage seen at the TS1/TS3 pins of the BQ76952. This is difficult to achieve as we have observed the voltage divider network is completed and the temperature is sampled for only about 10ms of the 126ms cycle time for volt/temp/current acquisiton. Is there some way through the configuration registers to ensure the switch that closes the voltage divider network for temperature measurements is *always* closed so a DMM applied to the TSx pins is able to get an accurate measurement of what is measured over the 103AT?