Tool/software:
Hello Team,
Need quick response for below topic,
I couldn't get a clear answer to the following statements from your feedback,
“In this situation, the SENSE voltage is applied to the IC before reaching the VDD POR threshold of 700mV, which is the specified minimum for proper operation. While I agree that this may fall within an "Undefined" region of the IC's operation, it's important to note that the datasheet does not specify that this behavior is "Forbidden." Therefore, this is not the cause of the abnormal behavior.
According to the datasheet timing diagram below and the configuration used in our application (CTR Open or NC), the IC's reset should go high within 380µs (Max Delay), based on the datasheet values (tSTART = 300µs max + tD = 80µs max) even SENSE signal applied before VDD supply.
Thank you