This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: GPC-report it's empty.

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: GPCCHEM

Tool/software:

Hello;

I need to test CHEMID, but the GPC-report obtained by uploading data through GPCCHEM is empty. I re-uploaded the data from the GPC-report I obtained before, but there was still no data.

The attachment <roomtemp_rel_dis_rel 1> is the newly learned data. <roomtemp_rel_dis_rel 1-1> is the previously learned data, and <GPC_report 1-1> is the previously obtained report. <roomtemp_rel_dis_rel 1-report> is the latest obtained report.

Website for uploading data     https://www.ti.com/powercalculator/docs/gpc/gpcUpload.tsp

roomtemp_rel_dis_rel 1.ziproomtemp_rel_dis_rel 1-1.ziproomtemp_rel_dis_rel 1-report.zip

Chemistry ID selection tool, rev=2.54		
		
Configuration used in present fit:		
ProcessingType=2		
NumCellSeries=1		
ElapsedTimeColumn=0		
VoltageColumn=1		
CurrentColumn=2		
TemperatureColumn=3		
		
Best chemical ID : 4103	Best chemical ID max. deviation, % : 6.28	
		
		
		
Summary of all IDs with max. DOD deviation below 15%		
		
Chem ID	max DOD error, %	Max R deviation, ratio
4103	6.28	2.94
400	6.75	5.76
414	9.85	1.25
448	10.03	0.76
445	10.91	0.65
6106	12.23	0.43
4184	14.07	5.67
4110	14.08	1.4
461	14.1	2.77
410	14.23	4.05
446	14.25	0.03
4171	14.31	2.17
4180	14.37	2.31
4195	14.52	2.09
4100	14.77	2.16
4111	14.79	0.63
417	14.92	3.01
		
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
		
		
Selection of best generic ID for ROM based devices like bq274xx		
		
		
Device / Family #1		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27411-G1C: 4.35V LiCoO2	34.72
3142	bq27421-G1D: 4.4V LiCoO2	35.55
128	bq27421-G1A: 4.2V LiCoO2	36.46
312	bq27421-G1B: 4.3V LiCoO2	37.23
Best generic ID 354		
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
		
		
Device / Family #2		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	34.72
1202	bq27621: (default) 4.2V LiCoO2	37.66
1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	43.09
Best generic ID 354		
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
		
		
Device / Family #3		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
3230	bq27426: (default) 4.35V LiCoO2	28.68
3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	35.55
1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	37.66
Best generic ID 3230		
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule