This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1046EVM: TUSB1046EVM testing along with power delivery for 15W (5V@3A, 9V@3A)

Part Number: TUSB1046EVM
Other Parts Discussed in Thread: TPS65987

Tool/software:

1. Hi i am using TUSB1046EVM INT053 Rev F .  I have connected this EVM board from Computer Board (COMe type 6) or  PC to a display monitor working fine for DP only Mode.

SETUP: COMe module--> DP cable -->P3/J3 of TUSB1046EVM--> USB-C to HDMI cable converter--> HDMI cable to Monitor: working fine can you please provide the same default Flash image file which was loaded in the TUSB1046EVM's to flash and test in another my custom board for DP only test???

2. I have an additional requirement adding to this TUSB1046 EVM TUSB1046EVM TUSB1046 USB Type-CTm Enabler Evaluation Module (Rev. A) in my design i.e  programmable PD for 5v to 9V switching is required based on sink device demand.  for this I have added the circuitry of the design  of EVM TIDA05-0012 :Power DUO Source 200 W USB-C PD Reference Design .

to Configure variable Voltage I have followed the same pinouts for PDO_0 and PDO_1 as it is in the EVM TIDA05-0012 :Power DUO Source 200 W USB-C PD Reference Design . but not other pins example 5V_PB and 9V_PB and  Buttons are not used. in this case Can i configure my PD chip TPS65987DH using the online tool TPS6598X-CONFIG IDE, configuration, compiler or debugger | TI.com for DP alt mode and variable power delivery application for 5v and 9V  as in my schematics snaps attached below.???? if not possible to use the Config tool we need to write firmware our own for TPS65987DH?? will it be possible ??