Part Number: TPSM843521
Tool/software:
Hello,
The TPSM843521 datasheet doesn’t list a maximum capacitance. Could you confirm that there isn’t a maximum capacitance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPSM843521
Tool/software:
Hello,
The TPSM843521 datasheet doesn’t list a maximum capacitance. Could you confirm that there isn’t a maximum capacitance?
Hi Lucas,
Depending on the application 100uF should suffice.
Regards,
Gautam
Gautam,
Is 100uF the maximum allowable capacitance on the output of this device?
There is no max recommendation, and you can use as per your application requirement.