This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601-SP: Unused pin of TPS50601-SP

Part Number: TPS50601-SP


Tool/software:

Hello.

If the SS, PWRGD, and EN pins function are not used, is it okay to use these pin open?

Please advise me.

koji

  • Hi Koji-san,

    Regarding the PWRGGD and EN pins, it is okay to leave them open if not used. PWRGD is an open-drain output, and EN is internally pulled up.

    It is not recommended to float the SS pin. A  SS capacitor should on the pin, as described in the device datasheet, to limit inrush current during device startup and avoid noise coupling into the pin during operation.

    Thanks,

    Andy