Other Parts Discussed in Thread: TPS1H100-Q1
Tool/software:
Dear TI Support Team,
We are currently evaluating the TPS7H2140-SEP device for use in a high-reliability application where output short-circuit protection and repetitive fault endurance are critical.
We have reviewed the datasheet and application notes, but would like to confirm the following points:
1. **Short-Circuit Endurance**:
Does the TPS7H2140-SP device undergo any internal or external qualification testing (e.g., based on AEC-Q100-012 or similar) for repetitive short-circuit conditions?
- If so, how many ON/OFF thermal protection cycles (via thermal swing or thermal shutdown) can the device withstand without degradation?
2. **Comparison with Other TI Devices**:
We have seen documentation (e.g., SLVA709A) for other TI devices like TPS1H100-Q1 that have passed AEC-Q100-012 with 1 million+ short-circuit cycles.
- Can we consider similar robustness for the TPS7H2140, even though it is not a Smart Power Switch?
3. **Failure Criteria**:
In case of prolonged operation under repetitive short-circuit conditions (e.g., output shorted with ~57.6W power loss), is there an expected degradation mode or time-to-failure characterization?
If you could provide relevant test data, design margin considerations, or guidance on usage limits for high-repetition short-circuit conditions, it would be greatly appreciated.
Best regards,