Part Number: BQ25798
Other Parts Discussed in Thread: LP2951, LM117
Tool/software:
I wanted to find out if this part is suitable for my use case, or if there is another part that would be better suited.
Use case:
12v - 24v DC input. 25W power supply, so 2.5A @ 12V.
12v DC system voltage
3S LiFePO4 cells, 3.2V each, 9.6V total, needs ~10.8V for charging.
The battery is external and can be unplugged hot, but it will almost never be done.
The battery is for backup if power is lost, thus 99.9% of the time it will be running off the DC Input power. If power is lost, it must be able to continue running off the battery without power interruption.
There is no need for fast battery charging; ideally, charging will be done at 100mA or less.
Currently, my design has a 12V-24V -> 10.8V buck converter, which then boosts the 10.8V and/or the battery voltage back to 12V. With the BQ25798 am I able to get rid of both of these circuits? I.E. The BQ25798 can take 12V - 24V DC input and then provide a stable 12V system voltage, in addition to the 10.8V that the batteries need for charging?