This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A96: regarding Softstart

Part Number: TPS7A96
Other Parts Discussed in Thread: TPS7A94, TPS7A57

Tool/software:

Dear Team,

TPS7A96
TPS7A94
TPS7A57

For the above mentioned parts 


to determine the softstart,The terms are given without any units in datasheets, Please refer the attached image
Please Guide me with determining the softstarts for 

The input Output voltages and Currents and are given below

Part Number TPS7A57 TPS7A57 TPS7A96 TPS7A94 TPS7A96
Selected Regulator Type LDO Regulator LDO Regulator LDO Regulator LDO Regulator LDO Regulator
Selected Regulator's Maximum output current (A) 5 5 2 1 2
Typical Output Voltage of Selected Regulator - Vo (V) 0.925 0.925 1.8 1.8 3
Planned Input Voltage of Regulator - Vi (V) 1.2 1.2 2.5 2.5 3.3
Required Output Current of Regulator - Io (A) 2.7636 3.9684 1.4736 0.4068 0.8592
Calculated Input Current of Regulator - Ii (A) 2.7636 3.9684 1.4736 0.4068

0.8592

Soft start time Tss (ms)

Please help me with filling the Tss,

Thanks and regards, 
Maharajan P