Hello,
Customer is using the TPS61081 for LED backlight control, using Fig 24 in the datasheet. They would like to know if there is a recommended FET for the PWM dimming?
Thanks in advance,
Mohammed
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Customer is using the TPS61081 for LED backlight control, using Fig 24 in the datasheet. They would like to know if there is a recommended FET for the PWM dimming?
Thanks in advance,
Mohammed
There is no recommendation. I suggest a FET with turn on speed at least 100x faster than your PWM signal. Also, I suggest adding 10 ohm resistor in series the FET's gate to prevent any ringing/overshoot at the gate. Also, I suggesting placing at least a 100 ohm resistor in series with the drain so that the SS pin is not pulled completely to ground.
I am sorry. I was not clear. In Figure 24, the circuit is switching between ILED(high) = I(ss) * R1 / Rset and ILED(low) = I(ss) * (R1||R2) / Rset. Alternatively, you could switch between ILED(high) = VFB / Rset and ILED(low) = I(ss) * R2 / Rset, where I(ss)*R2 < VFB and R1 is not used. If ILED(low) is supposed to be 0, then I recommend R2 be 10-100 ohm so that the SS pin is not pulled completely to ground.