TPS62067 Pre-Biase and soft start up Question.
TPS62067 Datasheet don't mention Pre-Biase function.
Is TPS62067 Pre-Biase function?
Load sink case, TPS62067 soft start up without problem?
Regard.
Bob Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS62067 Pre-Biase and soft start up Question.
TPS62067 Datasheet don't mention Pre-Biase function.
Is TPS62067 Pre-Biase function?
Load sink case, TPS62067 soft start up without problem?
Regard.
Bob Lee
This is a great question, so I made a design note for it here: http://e2e.ti.com/support/power_management/non-isolated_dcdc/w/design_notes/1679.aspx
Let me know if that doesn't answer your question.
Dear Chris Glaser
Thank you very much for your answer.
May I ask one more question?
Will you teach me TPS60k product which Pre-biased function is in.
Regard.
Bob Lee
We have a lot of TPS6k parts. It is best to find an IC that meets your power requirements and then see if that particular one supports a pre-biased output.
What are your power requirements?
Dear Chris Glaser
I want to safety soft start up device, in laod sink case.
TPS62067 include Pre-biased function, I felt relieved.
I would very much appreciate receiving your comment.
Regard.
Bob Lee
I'm sorry but I do not understand what 'load sink case' means? Could you re word this question?
If you can provide your input voltage, output voltage, and output current needs, I can recommend a suitable part that meets your requirements.
Dear Chris Glaser
I'm sorry.
'Load sink case' means current sink from output to IC.
TPS62067 include Pre-biased start up function.
I think that TPS62067 is safe.
Thank you for thinking about a recommend device.
Specification is input voltage 3.3V, output voltage 1V, output current 1.5A.
May I use TPS62067?
Or will you recommend other device?
Regard.
Bob Lee
Dear Chris Glaser
Thank you very much for teaching TPS62067 in various ways.
Regard.
Bob Lee