Tool/software:
Hi Sir,
What is the Ta(Ambient Temperature) range of TPS7A8401A ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Sir,
What is the Ta(Ambient Temperature) range of TPS7A8401A ?
Hi Kevin,
You can consider the junction temperature range to be the same as the ambient temperature range. However, any device heating will eat into the acceptable ambient range. For example, if the device was used to source a very small amount of current, the device could theoretically be used at an ambient temperature near 125C, but with more power dissipation the ambient temperature would need to be lower to keep the junction temperature under 125C.
Regards,
Nick