This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4800-Q1: Short circuit current set

Part Number: TPS4800-Q1

Tool/software:

Hello team 

for setting a Isc of 15A with sensing resistor of 2m ohms, RISC is coming around 5.5k, but the evaluation board having 10k, Why this much of variation ?

  • Anoop,

    The pink labels on the EVM are incorrect. The formula, for preproduction silicon that is not longer available, had 10mV as the constant voltage offset in the equation. While we updated the datasheet to reflect the new current limit values, the new values in the EVM should be 9.5A, 14.2A, and 19.5A. We are working on updating the EVM documentation now. 

    Best Regards,
    Tim