This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1211-Q1: Device behavior when Rshunt or CS+/- short condition

Part Number: TPS1211-Q1


Tool/software:

Hello Expert,


I want to make sure about behavior of device.


What will it happen when Rshunt or CS+/- shorted?

I suppose that it only cause disable of IMON and OCP but it won't lead disable of Pass FET.

Best regards,
Kazuki Kuramochi

  • Hi Kazuki-san, 

    Do you mean if Rshunt is shorted to CS+/-? Could you provide a picture? 

    I'm not sure I'm capturing your question so let me give a few pointers. 

    RSET between RSHUNT and CS+ is required to limit current to GND. 

    To properly disable SCP you must connect ISCP to CS-. This gauntness the voltage at SCP does not trigger SCP threshold set by RISCP. 

    The difference between CS+/- cannot exceed 0.3 V so you must also consider this or you will damage device. 

    To disable OCP you just need to connect IWNR directly to GND. 

    Thanks, 

    Sarah

  • Hi Sarah-san,

    My questions is just for what behavior will it happen during abnormal condition for debugging.
    I don't intend to disable OCP by the connection.

    What is the expected behavior which is caused by following short condition as written by red line and blue line below?

    Best regards,
    Kazuki Kuramochi

  • Hi Kazuki-san, 

    If you do not have an RSNS resistor as shown with red line then there will theoretically be no sensing. But at the same time you would probably be very susceptible to noise so you may see false ISCP triggers. 

    If CS+/- is shorted as shown on blue line similar behavior could be expected, but its important to note that the RSET is required to limit current on CS+. Ideally connecting CS+/- to one another guarantees that the two pins are kept at the same voltage and therefore the comparator will not trigger anything. 

    Thanks, 

    Sarah

  • Hi Sarah-san,

    I want to make sure about whether there is the other risk from this condition.

    Is there risk of disabling device's operation or cause damage from this situation?

    Best regards,
    Kazuki Kuramochi

  • Hi Kazuki-san, 

    Yes there is risk. You will not have working current protections in this configuration and may also experience false FLT LOW, which will shut off the device. 

    Thanks, 

    Sarah