Other Parts Discussed in Thread: BQ25798, USB-PD-CHG-EVM-01, TPS25751, , BQ34Z100
Tool/software:
Hi,
My needs:
- Design of a power backup system with 4 cells lithium battery (16850).
- USBC PD for the charge. The system must be fonctionnal if only 5V is available.
- Cells balancing and fuel gauge.
My researches:
- The USB-PD-CHG-EVM-01 ( TPS25751 and BQ25798) seems to be a good start for the first two points.
- The BP41Z50EVM seems to be a good idea for the last point.
Diagram with my ideas:

My questions:
- Is my diagram OK or have you better ideas ?
- The TPS25751 is configured by an external eeprom and this chip can configure the BQ25798 via dedicated IIC link: i'am right ?
- For the BQ41Z50 i'am lost: how to configure it ?
- By flashing a specific firmware ?
- There is an embedded eeprom memory ?
- Something else ?
Thanks for you help.
Best regards.