Other Parts Discussed in Thread: TPS61033, , TPS610333
Tool/software:
Hi, the datasheet for TPS61033 states "Up to 90.78% efficiency at VIN = 3.3V, VOUT = 5V, and IOUT = 2A" - the TPS61033EVM datasheet states it can do 1A max but the schematic indicates it could do 3A max under a high Vin... however testing on the bench, we can't get more than 1.2A from the EVM or my design with a 0.47uH inductor 3.7V to 5V. (or 1.5A from 4.7V in)
if this part is advertised at being able to do 2A out from 3.3V to 5V, is there any known/proven design for that capability?