This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25628E: Inductor sizing and current queestion

Part Number: BQ25628E


Tool/software:

Hi! I am pretty new to switching battery chargers, and have a design in which I'd like to try out the BQ25628E. 

In the "Inductor Selection" section of the datasheet for this part, there's mention of using I_chg for calculating the ripple and saturation currents needed to pick an inductor part. But, if I understand this part correctly, it is able to both charge a battery AND power a system simultaneously...is that right? If so, wouldn't I have an I_chg (the current being used to charge the battery) and - at times - I_sys (the current being used separately to power the system)? And, if so, would I then want to use the sum of these two currents to calculate inductor size? 

I'm sure this is a pretty entry-level question, I'm just a little confused why the datasheets seems to assert that I_chg is sufficient and complete for calculating saturation current. 

Thanks so much!

  • Hello, 

    Thank you for reaching out via E2E. Please see my comments below. 

    And, if so, would I then want to use the sum of these two currents to calculate inductor size? 

    You are correct that you will want to consider the total output current expected in your system when deciding the required saturation current for the inductor you select. Total output current will be ISYS plus ICHG. 

    Additionally, for your information the BQ25628E is designed to work with an inductor in range of 1uH to 2.2uH and then you have more flexibility when considering DCR and saturation current requirement of the inductor. A lower DCR inductor will result in better efficiency.

    You can also start by referencing the inductor used on our BQ25628EVM board. I have linked the user guide, which includes BOM for the board below. 

    https://www.ti.com/lit/ug/sluucq9/sluucq9.pdf 

    Best Regards,

    Garrett

  • Amazing, so super helpful. Thank you so much!