This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM60430-Q1: Request for Confirmation on ESR Suitability of Capacitor Used at LM60430-Q1 VCC Pin

Part Number: LM60430-Q1

Tool/software:

Hello,

I am writing to inquire about the capacitor used for the VCC pin of the LM60430-Q1. Specifically, we have used Taiyo Yuden's MCASE168SB7105KTNA01 (1uF / 1608 / 16V / X7R) for this purpose, as highlighted by the red box in the attached image.

Could you please confirm whether the ESR value of this capacitor is appropriate for use on the VCC pin of the LM60430-Q1?

We would appreciate your confirmation and any additional guidance you can provide.

Thank you and best regards.

  • Hi Donghyun,

    This device should be okay.

    You can even consider using a smaller package for the Capacitor (Like 0603). As long as you use a ceramic cap of the right capacitance value (and it is high quality - like X7R) - you should be fine. 

    Thanks,

    Best Regards,

    Taru