This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481-Q1: LM3481-Q1 Ton time specification

Part Number: LM3481-Q1

Tool/software:

In my application, input is 5V to 18V, my output is 11.64V, my duty cycle when Vin>8V is 34% & below, so Ton time =below 377ns when switching frequency is 917KHz, so what is the behavior of the output when it is below the minimum on time specification.?