Tool/software:
Hello TI community,
I have a few questions regarding the BQ25798 device. We are using this IC to charge a 2S custom-built battery pack for one of our new products.
Question 1:
p. 33 the of the BQ25798 datasheet (doc SLUSDV2B revised Jan. 2023) says :
“The host can monitor the ADC BAT pin voltage and TS fault register to determine when a valid battery is attached.”
We might have missed it but §9.5.1 (Resgister map) doesn’t mention such a register (REG20 and REG21 fault registers do not seem to have a “TS fault” field either). Could you please provide us with more details about this “TS fault” register ?
Question 2:
Assuming the BQ IC is charging the battery (i.e. CHG_STAT of REG1C is either 1h, 2h, 3h or 4h), what is the value of CHG_STAT (REG1C) when one of the charging timers (trickle, pre-charge, fast charge) expires? Does CHG_STAT roll back to 0h (not charging) ?
Question 3:
Assuming the BQ IC is charging the battery, when a VBUS over-voltage (VBUS_OVP), VBAT over-voltage or IBUS over-current (IBUS_OCP) condition occurs, which value does CHG_STAT (REG1C) take ?
Question 4:
When a VSYS over-voltage condition occurs, is VSYS supplied from the battery ? If the battery was charging, which is the new value of CHG_STAT once VSYS_OVP_STAT is set (indicating the over-voltage situation) ?
Question 5:
Assuming the battery is charging, what is the value of CHG_STAT when TS temperature goes higher than T5 (TS_HOT condition) or lower than T1 (TS_COLD condition) ? Can you please confirm that charging is suspended in those cases ?
Question 6:
When a TSHUT_STAT condition occurs, can you please confirm that battery charging is suspended ? In such a case, what is the value at VSYS ? If battery charging was ongoing, what is the value of CHG_STAT once TSHUT_STAT is set ?
Many thanks in advance for you support
Kind regards
Romaric