Other Parts Discussed in Thread: LP5912
Tool/software:
Hi team,
Does TPS736 (ADJ output version) have new gen or can you help recommend other LDO like TPS736 with reverse current protection but has lower Iq and higher PSRR?
BR
Amber
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Amber,
Another option would be LP5912 for reverse current and lower IQ, however this device only comes in fixed output. Is this roughly what you were looking for as an alternative?
LP5912 | TPS736 | |
Iout(Max)(A) | 0.5 | 0.4 |
Vin(Max)(V) | 6.5 | 5.5 |
Vin(Min)(V) | 1.6 | 1.7 |
Vout(Max)(V) | 3.3 | 5.4 |
Vout(Min)(V) | 0.9 | 1.2 |
Fixed output options(V) | 0.9, 1, 1.1, 1.2, 1.5, 1.8, 2.5, 2.8, 3, 3.3, 5 | 1.25, 1.5, 1.6, 1.8, 1.9, 2.5, 3, 3.2, 3.3, 4.3 |
PSRR @ 100 KHz(dB) |
40 | 32 |
Noise(uVrms) | 12 | 30 |
Accuracy(%) | 3 | 1 |
Dropout voltage (Vdo)(Typ)(mV) |
150 | 75 |
Iq(Typ) (mA) |
0.03 | 0.4 |
Output capacitor type | Ceramic | Cap Free, Ceramic |
Thermal resistance θJA(°C/W) |
71 | 53 |
Operating temperature range(C) |
-40 to 125 | -40 to 125 |
Package size: mm2 | 4 mm2: 2 x 2 (WSON|6) | 9 mm2: 3 x 3 (SON|8), 23 mm2: 3.5 x 6.5 (SOT-223|6), 5 mm2: 1.6 x 2.9 (SOT-23|5) |
Regards,
Andres