Tool/software:
Hi TI Team,
I am planning to use TPS53681 + 3x CSD95410 solution for my design to power the SoC core voltage.
Below are my design requirements:
Input voltage: 12V
Output voltage: 0.75V
Output current: 60A
I would like to know the following details based on the above specifications.
1. Whether TPS56381 + 3x CSD95410 solution can support here?
2. What is the default output voltage set from the factory?
3. Is there options to control the output voltage at the initial power ON to save my SoC from damage if the default factory set voltage is different from my required voltage?
4. What is the MP and support status for both the chips?
5. Whether heat sink is required for my application?
6. Is that fine if I am using only one output voltage configuration
Also please let me know if there are any other better solutions which is suitable for my application.
Regards
Shyam