This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80 LED question

Part Number: BQ40Z80


Tool/software:

When the battery is fully charged to 100%, the four configured LED lights will all turn on. They should normally remain constantly lit, but at this moment, two of the LEDs are slightly blinking at a slightly faster frequency.How should I configure it so that they remain constantly lit when the battery is fully charged instead of having two lights flashing ?

Looking forward to your reply. Thank you.

 4621.bq40z80 data memory.gg.csv

Mon Jun 16 18:39:41 CST 2025

Device Version Info = 4800_0_04
BQZ Device Name = bq40z80
BQZ Firmware Version = V0_04_BLD5

Design Capacity = 6200
Design Voltage = 14800
Specification Info = 0x0031
Manufacturer Date = 2023-12-19
Serial Number = 0x0001
Manufacturer Name = Texas Instruments
Device Name = bq40z80
Device Chemistry = LION

Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,CellVolt5,CellVolt6,CellVolt7,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellCurr5,CellCurr6,CellCurr7,CellPower1,CellPower2,CellPower3,CellPower4,CellPower5,CellPower6,CellPower7,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,RaScale5,RaScale6,RaScale7,CompRes1,CompRes2,CompRes3,CompRes4,CompRes5,CompRes6,CompRes7,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,CellGrid5,CellGrid6,CellGrid7,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0_5,DOD0_6,DOD0_7,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,DODEOC_5,DODEOC_6,DODEOC_7,QMax1,QMax2,QMax3,QMax4,QMax5,QMax6,QMax7,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxDOD0_5,QMaxDOD0_6,QMaxDOD0_7,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,RawDOD_5,RawDOD_6,RawDOD_7,CBTime1,CBTime2,CBTime3,CBTime4,CBTime5,CBTime6,CBTime7,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBDOD_5,CBDOD_6,CBDOD_7,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus
1,2025-06-16 18:39:42,1.001,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16700,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4174,4176,0,0,0,16699,16504,-9,-9,-8,-7,0,0,0,-4,-4,-3,-3,0,0,0,-13,-13,25.7,26.2,196.4,-273.2,-273.2,26.2,25.7,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,126,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1177,SUCCESS
2,2025-06-16 18:39:43,2.195,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16700,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4174,4175,0,0,0,16700,16503,-9,-10,-9,-7,0,0,0,-4,-4,-4,-3,0,0,0,-13,-13,25.8,26.2,196.5,-273.2,-273.2,26.2,25.7,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,127,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1158,SUCCESS
3,2025-06-16 18:39:44,3.368,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16699,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4175,4176,0,0,0,16699,16504,-8,-8,-8,-8,0,0,0,-3,-3,-3,-3,0,0,0,-13,-13,25.8,26.2,196.4,-273.2,-273.2,26.2,25.8,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,129,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
4,2025-06-16 18:39:46,4.929,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16700,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4175,4176,0,0,0,16697,16507,-7,-9,-8,-5,0,0,0,-3,-4,-3,-2,0,0,0,-13,-13,25.7,26.2,196.5,-273.2,-273.2,26.2,25.7,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,130,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1141,SUCCESS
5,2025-06-16 18:39:47,6.088,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16699,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4175,4176,0,0,0,16699,16505,-10,-8,-8,-8,0,0,0,-4,-3,-3,-3,0,0,0,-13,-13,25.8,26.2,196.5,-273.2,-273.2,26.2,25.8,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,131,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1155,SUCCESS
6,2025-06-16 18:39:48,7.258,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16699,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4174,4176,0,0,0,16697,16504,-7,-9,-9,-9,0,0,0,-3,-4,-4,-4,0,0,0,-13,-13,25.8,26.2,196.5,-273.2,-273.2,26.2,25.8,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,133,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1170,SUCCESS
7,2025-06-16 18:39:49,8.834,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16700,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4175,4176,0,0,0,16697,16508,-8,-8,-8,-4,0,0,0,-3,-3,-3,-2,0,0,0,-13,-13,25.8,26.2,196.5,-273.2,-273.2,26.2,25.8,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,134,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1160,SUCCESS
8,2025-06-16 18:39:51,10.010,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16700,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4175,4175,4175,0,0,0,16700,16504,-9,-8,-9,-8,0,0,0,-4,-3,-4,-3,0,0,0,-13,-13,25.8,26.2,196.5,-273.2,-273.2,26.2,25.8,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,135,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,0,0,0.95,9748,88,80,80,72,0,0,0,0,2049,2056,3591,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1155,SUCCESS
9,2025-06-16 18:39:52,11.181,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16735,161,161,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18739,-24800,-12400,100,0x0187,0x0000,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4185,4188,0,0,0,16745,16555,370,367,368,369,0,0,0,155,154,154,155,0,0,0,589,269,27.0,26.2,196.3,-273.2,-273.2,26.2,25.7,26.2,6420,9389,6320,9224,6926,6420,9389,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,0,88,80,80,72,0,0,0,0,0,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2047,2056,3589,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1155,SUCCESS
10,2025-06-16 18:39:53,12.352,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16745,375,175,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4184,4187,0,0,0,16778,16592,376,377,372,372,0,0,0,157,158,156,156,0,0,0,630,293,27.7,26.2,196.5,-273.2,-273.2,26.2,27.5,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,2,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2046,2056,3588,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1154,SUCCESS
11,2025-06-16 18:39:55,13.914,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16745,374,188,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4186,4184,4188,0,0,0,16771,16590,372,373,371,369,0,0,0,156,156,155,155,0,0,0,625,336,28.6,26.2,195.6,-273.2,-273.2,26.2,28.6,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,3,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2045,2056,3587,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1172,SUCCESS
12,2025-06-16 18:39:56,15.103,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16745,370,212,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4184,4188,0,0,0,16778,16585,368,367,367,367,0,0,0,154,154,154,154,0,0,0,618,354,29.0,26.2,196.4,-273.2,-273.2,26.2,28.9,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,4,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2043,2056,3585,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1172,SUCCESS
13,2025-06-16 18:39:57,16.290,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16746,367,222,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4184,4188,0,0,0,16779,16595,365,363,364,363,0,0,0,153,152,152,152,0,0,0,613,372,29.2,26.2,196.4,-273.2,-273.2,26.2,29.2,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,6,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2042,2056,3584,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
14,2025-06-16 18:39:59,17.851,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16746,363,232,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4184,4188,0,0,0,16773,16593,361,360,360,358,0,0,0,151,151,151,150,0,0,0,606,402,29.6,26.2,196.4,-273.2,-273.2,26.2,29.6,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,7,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2041,2056,3583,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1140,SUCCESS
15,2025-06-16 18:40:00,19.008,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16746,361,248,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4185,4188,0,0,0,16780,16588,356,358,357,358,0,0,0,149,150,149,150,0,0,0,601,416,29.8,26.2,196.5,-273.2,-273.2,26.2,29.7,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,8,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2040,2056,3582,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
16,2025-06-16 18:40:01,20.181,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16746,358,256,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4185,4189,0,0,0,16780,16589,355,356,355,355,0,0,0,149,149,149,149,0,0,0,598,428,30.1,26.2,196.5,-273.2,-273.2,26.2,29.9,26.2,6421,9390,6320,9224,6927,6421,9390,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,9,88,80,80,72,0,0,0,-1,-1,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-1,0,0.95,9748,88,80,80,72,0,0,0,0,2038,2056,3580,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
17,2025-06-16 18:40:02,21.741,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16747,355,262,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18740,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4186,4185,4189,0,0,0,16774,16594,352,351,350,352,0,0,0,147,147,146,147,0,0,0,591,449,30.3,26.2,196.5,-273.2,-273.2,26.2,30.1,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,11,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2037,2056,3579,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1128,SUCCESS
18,2025-06-16 18:40:04,22.883,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16748,352,268,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4186,4185,4188,0,0,0,16774,16595,348,351,350,351,0,0,0,146,147,146,147,0,0,0,588,459,30.4,26.2,196.5,-273.2,-273.2,26.2,30.4,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,12,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2036,2056,3578,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1157,SUCCESS
19,2025-06-16 18:40:05,24.057,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16749,350,279,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,4185,4189,0,0,0,16774,16590,347,349,346,348,0,0,0,145,146,145,146,0,0,0,585,467,30.5,26.2,196.5,-273.2,-273.2,26.2,30.5,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,13,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2035,2056,3577,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1153,SUCCESS
20,2025-06-16 18:40:06,25.620,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16748,347,284,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4187,4186,4189,0,0,0,16781,16598,344,344,343,344,0,0,0,144,144,144,144,0,0,0,579,482,30.7,26.2,197.4,-273.2,-273.2,26.2,30.7,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,15,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2033,2056,3575,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1171,SUCCESS
21,2025-06-16 18:40:07,26.808,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16748,345,288,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4187,4186,4189,0,0,0,16775,16598,341,342,342,343,0,0,0,143,143,143,144,0,0,0,575,488,30.8,26.2,196.4,-273.2,-273.2,26.2,30.8,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,16,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2032,2056,3574,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1152,SUCCESS
22,2025-06-16 18:40:09,27.978,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16749,343,291,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4187,4185,4189,0,0,0,16775,16592,338,341,340,340,0,0,0,142,143,142,142,0,0,0,571,494,31.0,26.2,196.3,-273.2,-273.2,26.2,30.9,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,17,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2031,2056,3573,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1171,SUCCESS
23,2025-06-16 18:40:10,29.553,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16749,340,298,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16782,16598,337,337,338,338,0,0,0,141,141,141,142,0,0,0,568,503,31.1,26.2,196.5,-273.2,-273.2,26.2,31.1,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,19,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2029,2056,3571,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1157,SUCCESS
24,2025-06-16 18:40:11,30.728,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16749,339,301,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4187,4186,4189,0,0,0,16775,16597,335,335,336,336,0,0,0,140,140,141,141,0,0,0,565,507,31.2,26.2,196.8,-273.2,-273.2,26.2,31.1,26.2,6422,9392,6320,9224,6928,6422,9392,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,20,88,80,80,72,0,0,0,-2,-3,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-2,0,0.95,9748,88,80,80,72,0,0,0,0,2028,2056,3570,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1157,SUCCESS
25,2025-06-16 18:40:13,31.901,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16750,337,303,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16776,16598,336,336,336,335,0,0,0,141,141,141,140,0,0,0,563,511,31.4,26.2,196.0,-273.2,-273.2,26.2,31.4,26.2,6423,9393,6320,9224,6928,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,21,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2027,2056,3569,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1153,SUCCESS
26,2025-06-16 18:40:14,33.459,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16750,334,307,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16783,16598,333,331,331,331,0,0,0,139,139,139,139,0,0,0,558,517,31.3,26.2,196.5,-273.2,-273.2,26.2,31.3,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,23,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2025,2056,3567,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1159,SUCCESS
27,2025-06-16 18:40:15,34.633,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16750,332,309,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16783,16599,329,331,330,329,0,0,0,138,139,138,138,0,0,0,554,520,31.6,26.2,196.7,-273.2,-273.2,26.2,31.5,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,24,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2024,2056,3566,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1171,SUCCESS
28,2025-06-16 18:40:16,35.821,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16750,330,310,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16776,16597,327,327,327,330,0,0,0,137,137,137,138,0,0,0,553,522,31.6,26.2,195.7,-273.2,-273.2,26.2,31.6,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,25,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2023,2056,3565,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1140,SUCCESS
29,2025-06-16 18:40:18,37.368,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16751,328,313,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16784,16605,325,327,326,325,0,0,0,136,137,136,136,0,0,0,549,524,31.7,26.2,197.0,-273.2,-273.2,26.2,31.7,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,27,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2021,2056,3563,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
30,2025-06-16 18:40:19,38.539,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16751,327,314,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4190,0,0,0,16783,16599,323,324,326,323,0,0,0,135,136,136,135,0,0,0,546,527,31.8,26.2,196.4,-273.2,-273.2,26.2,31.8,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,28,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2020,2056,3562,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1156,SUCCESS
31,2025-06-16 18:40:20,39.714,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16751,325,315,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4190,4187,4186,4189,0,0,0,16776,16598,320,323,322,321,0,0,0,134,135,135,134,0,0,0,543,528,31.9,26.2,196.4,-273.2,-273.2,26.2,31.8,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,29,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2019,2056,3561,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1155,SUCCESS
32,2025-06-16 18:40:22,41.274,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16752,323,316,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,4186,4189,0,0,0,16783,16598,320,319,321,320,0,0,0,134,134,134,134,0,0,0,539,529,32.0,26.2,196.5,-273.2,-273.2,26.2,31.9,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,31,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2017,2056,3559,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1171,SUCCESS
33,2025-06-16 18:40:23,42.460,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16752,321,316,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4188,4186,4189,0,0,0,16785,16601,318,319,318,317,0,0,0,133,134,133,133,0,0,0,536,530,32.0,26.2,196.4,-273.2,-273.2,26.2,32.0,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,32,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2016,2056,3558,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1157,SUCCESS
34,2025-06-16 18:40:24,43.633,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16721,180,316,1,100,102,6320,6320,65535,65535,0,3000,16800,0x00A0,0,-32767,-18743,-24800,-12400,100,0x0187,0x1002,0x10,0x0008,0x12,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4178,4179,4179,4180,0,0,0,16748,16559,-6,-7,-8,-9,0,0,0,-3,-3,-3,-4,0,0,0,27,496,32.1,26.2,196.5,-273.2,-273.2,26.2,32.1,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,33,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2015,2056,3557,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1171,SUCCESS
35,2025-06-16 18:40:26,45.210,0x0187,300,10,0x6001,0,65535,65535,1,26.2,16713,-8,-8,1,100,102,6320,6320,47400,47400,65535,3000,16800,0x00E0,0,-32767,-18743,-24800,-12400,100,0x0187,0x0002,0x10,0x0008,0x52,0x0014,0x02B8,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4177,4179,4178,4179,0,0,0,16713,16522,-9,-8,-8,-8,0,0,0,-4,-3,-3,-3,0,0,0,-13,-13,30.5,26.2,196.4,-273.2,-273.2,26.2,30.9,26.2,6423,9393,6320,9224,6929,6423,9393,-100,-165,6320,9224,26.2,26.1,1000,1000,1000,1000,0,0,0,0,0,0,0,0,0,0,0,14,0,0,0,0,0,0,0,2,88,80,80,72,0,0,0,-3,-4,0,48,316,64,56,0,0,0,6990,6960,6991,6982,0,0,0,0,0,0,0,0,0,0,-3,0,0.95,9748,88,80,80,72,0,0,0,0,2015,2056,3557,0,0,0,88,80,80,72,0,0,0,16384,6337,9231,1158,SUCCESS