This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3050: BQ8050 output PWM3.3V abnormal in the high temperature

Part Number: BQ3050
Other Parts Discussed in Thread: BQ8050

Tool/software:

Hi TI engineer:

I have some questions about the BQ8050 IC using in the high temperature.The specific description as follows.

We use the BQ8050 RC6 Pin to output PWM3.3V,When the IC temperature is around 37℃ to 43℃, there is no PWM output. Then, when the IC temperature drops to around 34℃, the PWM output is normal

This issue is extremely urgent. I hope to receive a reply as soon as possible. Thank you!