This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26750: I2Ct read of Transmit Source Capabilities Register(0x32) registers not as I have programmed the EEPROM.

Part Number: TPS26750

Tool/software:

Hi There,

I am working on a project with a TPS26750 with support for 5 SPR PDO and one EPR PD up to 140W (28v @5A).

I have configured the firmware using the USBCPD Application Customization tool and programmed my board using a Aardvark programmer.

The board appears to be working as expected and I can selected the programmed PDOs and EPR and it outputs the correct voltages.

I want to be able to monitor and control the TPS26750 via the I2Ct interface but I am finding that when I read register 0x32 it doesn't have the same setting that I programmed the EEPROM with.

I have attached a logic analyser capture of the read from register 0x32, I am expecting that PDO and EPR (in bits 0-5) should be 5 and 1 respectively but they are coming out as 7 and 7. 

I suspect I am missing something, any assistance would be appreciated.

Thanks in advance

Regards

Erik

p.s. I don't appear to be able to upload the .sal file, I have tried on multiple browsers and computers.