Hi,
Could you please help clarify the SPLYGD (non-inverted) pin Vol level when not active in TPS259480AYWP.
This is an OD signal that is asserted high when the input supply is valid and the channel has completed the inrush sequence.
What should be Vol_max in the following cases?
How can I estimate the Strong or Weak PU values for Vol?
Is the Iq current +-3uA related to the active high state?
SPLYGD Vol=? VIN = 0V, Strong pull-up
SPLYGD Vol=? VIN >3.3V, Strong pull-up
SPLYGD Vol=? VIN >3.3V, Weak pull-up
SPLYGD Vol=? VIN <3.3V, Strong pull-up
SPLYGD Vol=? VIN <3.3V, Weak pull-up
I am sharing with you the implementation based on the SPLYGD signal and N-channel MOSFET with High Vgs_th.
Regards
Vitaliy