Tool/software:
HI TI
I want to use the BQ25798 to charge a 4S lithium battery. My circuit configuration is as follows: PROG is set to 17.4K, power input is VBUS 2 12V 1A, SYS output reaches VSYSMIN 12V, but when I connect the battery, I cannot measure 16.8V at the BAT PIN. I can see the STAT LED blinking, but when I read the FAULT STATUS via I2C, all values are 0. I want to know why all the read values are 0 and how to determine the reason why the IC cannot charge.