Tool/software:
Hi TI team,
We are in the process of freezing a design with a TPS7A20U regulator. We need your support with the thermal calculation to ensure that the IC does not exceed the Junction temperature maximum (Tjmax). We have done a calculation, which I have disclosed below. Can you please correct the calculation If I made any mistake in it?
Note: Kindly consider the PCBA designs are up to the mark and that all the design constraints are followed.
TPS7A20U | |||
Vin(V) | 5 | E4 | |
Vout(V) | 3 | E5 | |
Iout(A) | 0.1 | E6 | |
Iq(A) | 0.01 | E7 | |
Pd(w) | 0.21 | E8 | |
Tjmax(deg C) | 125 | E10 | |
Ta(deg C) | 25 | E11 | |
Rth | 476.1905 | Consider Tj =125, TA=25; (E10-E11)/E8 | E13 |
Tj | 140 | Consider 40 degC ambient; (E8*E13)+40 | E14 |
We have noticed that the maximum junction temperature in the datasheet is mentioned as 125degC. We want to know the TJ during TA= 50 degC, 60degC and 70degC
Regards,
Murugavel.S