Part Number: TPS65987DDK
Other Parts Discussed in Thread: TPD8S300, TPS65987
Tool/software:
Hello e2e,
I am working on finding the correct configuration for a device that should be alt mode capable. Forgive me, I am a beginner with the PD protocol. The device should primarily look to be a sink in the power context (UFP) and a source in the data/alt mode context (DFP_D). We are using the GPIO configuration. So far, we have been able to see the device sink, although it only negotiates for 5V even though it has been configured with 4 sink PDO's up to 20V. Our protocol analyzer shows a negotiation occur with several messages going back and forth. When we connect a display through an externally powered usb hub no messages appear to be going across. Another concern is that the same image when programmed onto one of the EVM's, appears to be functioning correctly on the EVM.
Please let me know what data you would like me to share. I can send the schematic in a private message.
Any assistance you can provide would be invaluable, thank you.