This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: Cross regulation : Multioutput Config 2 switch flyback vs 1 switch (standard)

Part Number: LM5023
Other Parts Discussed in Thread: PMP41031

Tool/software:

I was trying to design a multioutput flyback with Vin range : 100V to 700VDC and Vout : 18V, 5V, Pout : 65W (combined).

Is there a good reference material available to evaluate the cross regulation aspects of 2 switch vs 1 switch flybacks. I am presuming, the 2 switch flyback would be better as the Vclamp is limited to Vin. I have ordered the PMP41031 design from TI.

But if there are any suggestion/ materials for 2 switch flyback topology for multioutput versions which talk about cross regulation, that will really help.