This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5868: Steps to turn on the LED

Part Number: LP5868
Other Parts Discussed in Thread: LP5866

Tool/software:

Dear Sirs and Madams,

We created a PCB with an LP5868 mounted on it, but the LED is not lighting up.

LED Hardware Configuration : SW[0:5], CS[0:13]

interface : I2C mode (ADDR0, ADDR1 and IFS are connected to GND)

We tried to turn on one LED to check that the board was working, but after sending 'H' from VIO_EN from the external MCU, I issued the following command using the I2C interface, but the LED did not light up.

The steps we took to light up the L3-CS6 LED dots(1) CS Enable:

(1) CS enable

Write 0x01 to address 0x000

(2) Set Mode 1

Write 0x30 (=11 0000b) to address 0x003

110b : 6 scan lines 

00b : Mode1

0b : PWM freq is 125kHz

(3) "LED dot L3-CS6" set on

Write 0x40 (=0100 0000b) to address 0x04C

(4) PWM of "L3-CS6" is on (About duty 50%)

Write 0x80 (=1000 0000b) to address 0x23C

The LED current remains at the default 20mA.

Are there any other commands I need to do besides the steps above?

 

Regards,

Masashi