This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25820: Battery management, LiFePo4, IGBT, Drivers

Part Number: BQ25820


Tool/software:

Hello, I would like your professional opinion on the feasibility of implementing the sample conceptual circuit below. The goal is to charge one lithium-phosphate cell - 3.65V/300A at an input voltage of 12V/125A. I also have doubts about the stability of the circuit.

Best regards,

Tsvetan Ginin

  • Hello Tsvetan,

    Hello, I would like your professional opinion on the feasibility of implementing the sample conceptual circuit below. The goal is to charge one lithium-phosphate cell - 3.65V/300A at an input voltage of 12V/125A. I also have doubts about the stability of the circuit.

    The BQ25820 is not rated for 300A charging, the Max we recommend is 20A. it may be possible with multiple BQ25820 in parallel

    best Regards,

    Chrstian