Tool/software:
Hi AE,
1. If I set the current to 10mA and control the PWM with a 50% duty cycle, the average current will be around 5mA, correct?
2. If I want to set a constant current of 10 mA, I need to use a 7.35 kΩ resistor, right?
3. Imax depends on the Max_Current_Option bit to protect against IREF being shorted or left floating, right?

Best Regards
x