This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5861: Max input current on VIO_EN pin

Expert 1005 points
Part Number: LP5861

Tool/software:

I'm planning on just tying the VIO_EN pin high, but was wondering why the datasheet doesn't specify the VIO_EN current when active.
I'm guessing that my uController could supply enough current using a typical GPIO since that is what the LP5861 datasheet says it can connect to (with a 1000pF cap near the pin), but the 5uA seems minimal and not the correct value for the OE_ function when the part is being programmed.

Is there a GPIO max current spec for this input?