This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: Current limit for 0.5A

Part Number: TPS2595

Tool/software:

Hi,

A customer is using TPS259573 to limit the load current from a USB port at ~500mA.  The Vin is 5V, in case it matters.

I used the design calculator SLVC704A to determine Rilim.  The RILM_Cal value is 4020.10 Ohm (cell D36), but D37 is #REF!.  It appears to be because the Res EIA tables just don't extent far enough to show a 4KOhm value.  So is this as simple as selecting a resistor in the range of 4.0 to 4.3 kOhm, or is there some reason the tool doesn't provide resistor values this high?

Thanks,

Darren