Other Parts Discussed in Thread: EV2400, USB2ANY
Tool/software:
I have a problem with low voltage on REGN on my own custom PCB
I'm using a 7S battery and 20V input. I see the output switch from the battery voltage of 25V to 20V when the input is turned on. Status registers read over I2C show that Power is Good but that DRVSUP is out of range. Scoping the REGN signal shows that it goes from 0 to 250mV when power is turned on
14:08:38.310 -> 0x21: 0x8 ⇔ Reserved
14:08:38.310 -> 0x22: 0x80 => Power Good
14:08:38.310 -> 0x23: 0x2 - ACGET on
14:08:38.310 -> 0x24: 0x2 - DRVSUP out of range
Attached is my schematic.
Can you suggest any possible causes for the low voltage on REGN?
Best regards,
Phil