This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260: Please tell me about the forced output off.

Part Number: TPS54260

Tool/software:

Please tell me about the forced output off.

VIN = 5.0 V, BOOT-PH = 3.3 V
If the Vin of the TPS54260MDGQTEP is interrupted at room temperature, it may not output.
It often does not output at low temperatures.

The explanation of boot is as follows: the output is forced to switch off until the capacitor is refreshed.
Does it occur when boot>ph?