This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5926: seeking low noise led driver with I2C interface, no PWM

Part Number: TLC5926
Other Parts Discussed in Thread: TLC59108

Tool/software:

Dears, (I've indicated a particular IC part number in the subject, but my question is more general, thanks).

I'm working on an audio project, and I'm searching for LED drivers with no PWM, to avoid noise. I need one sink (common anode LEDs) and one 'voltage' (common cathode LEDs) driver. 

Could you please suggest two  drivers, which could comply with the following requirements please ?

- I2C interface to microcontroller

- no PWM, this is important

- SSOP or DIP form factor, if possible

- Sink driver: 8 channels, 50mA (for the RGB LEDs and two backlight leds as well)

- 'Voltage' driver: 4 channels, 50mA

- Power supply of the MPU will be 3.15V, hence logic levels will be accordingly

Thank you very much in advance !

Cheers

Matteo