Tool/software:
Hello expert, I would like to confirm the default output voltage of each power supply for the PTPS6521402VAFR PMIC chip. Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello expert, I would like to confirm the default output voltage of each power supply for the PTPS6521402VAFR PMIC chip. Thank you!
Hello Junzhi,
Here are the default output voltages for PTPS6521402:
PMIC Rail | Default Output Voltage |
BUCK1 | 0.75 V |
BUCK2 | 1.80 V |
BUCK3 | 3.30 V |
LDO1 | 1.80 V |
LDO2 | 2.50 V |
Best Regards,
Sarah
Hi Junzhi,
The above values are the default output voltages for PTPS6521402VAFR. (This is the same as PTPS6521402)
Let me know if you meant something else, or need additional help with this device.
Best Regards,
Sarah
Currently, I have obtained this PMIC and want to verify its output. However, upon actual measurement, it was found that when using this circuit for verification, the PMIC did not output anything. Only VPP1P8 had a voltage of 1.78V, while the other LX and LDO did not output anything. Is there a problem with this verification circuit? Could you please provide the simplest verification circuit? Thank you!
Hi Junzhi,
I do not notice any issues with the schematic. VDD1P8 showing 1.78 is a sign that PMIC is being powered on correctly.
The schematic in the TPS65214EVM user guide can be used as reference for verification circuit.
Are you able to capture the startup signals of VIN signal, EN, GPO, and BUCK2 pin on oscilloscope, if possible?
Can you also check if nRST pin is outputting HIGH or LOW?
Thank you,
Sarah
Hello, currently, the output of my verification is as follows: when the GPIO/VSEL pin is pulled up to 3.3V, BUCK1 is not 0.75V by default. May I ask what the reason is?
BUCK1:The output is variable.
BUCK2:1.8V
BUCK3:1.2V
LDO1:1.8V
LDO2:2.5V
Hi Junzhi,
What voltage does BUCK1 change to when GPIO/VSEL is HIGH?
Are you using I2C in your system, and are you able to provide the register readings?
Specifically, the values at addresses 0x01, 0x41, and 0x1F ?
This looks like Buck1 is configured as the VSEL rail for GPIO/VSEL pin,
but this should not be the case for PTPS6521402VAFR default settings, please help to share the register values if you are able, so I may confirm the reason for the issue here.
Best Regards,
Sarah
Currently, we are only conducting pure hardware verification and there is no connection to the SOC. The I2C signal has only been pulled up, and it has not been connected to the AM62Lx or any other SOC. The output waveform of BUCK1 is as follows and it is constantly adjusting in a loop.
BUCK2 and BUCK3 will not adjust again after stabilization. For example, the waveform of BUCK3 is as follows.
Hi Junzhi,
Thank you for sharing the waveforms. It may be harder to understand the problem without I2C readings, so I may have some more questions.
This initial oscillation is not normal for any of the outputs. The output should immediately be stable for BUCK2, BUCK3 .
Can you also share waveform for VSYS input, to see if it is noisy?
The outputs look to be picking up some higher voltage up to 2.8 V.
Are you able to share the layout? This can be shared over our email thread, if necessary.
Best Regards,
Sarah