Tool/software:
Hi TI
Please tell me how to select the constant Rz(comp pin).
What effect does increasing Rz have?
Also, are there any recommended upper or lower limits for Rz?
As shown below, we have confirmed that the reduction in output voltage during a sudden load change is smaller under condition B than under condition A.
We are considering increasing Rz, but are there any disadvantages to doing so?
・Condition A
Rz: 9.1kΩ
Cz: 2.2uF
Output voltage change during a sudden load change: 400V→350V→400V
・Condition B
Rz: 91kΩ
Cz: 0.22uF
Output voltage change during a sudden load change: 400V→370V→400V
Sudden load change: 0W→180W
best regards,