This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: BQ8050 PWM Output abnormal cause the discharge mos burned

Part Number: BQ4050
Other Parts Discussed in Thread: BQ8050

Tool/software:

Hi 

Customer use BQ8050, and found that its PWM output abnormal and caused the discharge mos burned during the aging test at around 43°C temperature. 

and when the temperature lower aound 30°C, the PWM output can recover and output normal.

I attached the schematic in the FA request  form, and the register parameter. Could you help check ? and I had summited FA at the same time.

Thanks

ZP22314-01项目BQ8050 配置信息-250618.zip

 TI FAR NEW FORM_BQ8050_20250618 (Update).docx