This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24298: System regulation in battery mode isn't happening at temperatures above 45 C.

Part Number: BQ24298

Tool/software:

We have a device utilizing the system output when VBUS is absent and only the battery is present. When the temperature exceeds 45 degrees Celsius, the system voltage is no longer regulated. Is there a register setting we need to address to correct this issue?

  • Hi,

    Could you please provide the following for room temp and 45C respectively? You mentioned VBUS is absent please confirm below.

    1. The charger operating conditions such as VBUS (voltage at VBUS pin), IVBUS, VBAT (voltage at BAT pin), IBAT, VSYS, ISYS.
    2. All the register readings. The register readings help to understand the charge operating status and fault conditions if any.

    Thanks,

    Ning

  • Issue was unrelated, no further action needed.