This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Using TPS25982 with 12V DC fan having peak current 19A

Part Number: TPS25982

Tool/software:

Hi Team 

We are using above part for controlling power on DC fan , typical current requirement is 9 Amp  , but peak current requirement is  19 Amp. I want  to understand 

if I will limit current  to 11Amp . what will be  behaviour of  IC  during start-up. 

1) Will it  keep on supplying 11Amp or it will turn off  ?

2) Based on application notes  SLVA683  TPS25982 can able  to  limit peak current requirements. But can you please  confirm if  same part  will  be okay in above configuration.